:NETWorks:TRACe:THReshold:GENeral:AUTO
Command Syntax
:NETWorks:TRACeN:THReshold:GENeral:AUTO
Where N identifies a specific trace and must be selected from 1 to 128 {1:128}.
Description
When you select the ± Hysteresis threshold definition for the selected signal (see :NETWorks:TRACe:THReshold:GENeral:METHod), you can send :NETWorks:TRACe:THReshold:GENeral:AUTO to automatically set the Center Threshold (:NETWorks:TRACe:THReshold:GENeral:MIDDle) to be halfway between Vmin and Vmax and the Hysteresis value (:NETWorks:TRACe:THReshold:GENeral:HYSTeresis) to be ±0.05(Vmax - Vmin).