:NETWorks:TRACe:THReshold:GENeral:STZero
Command Syntax
:NETWorks:TRACeN:THReshold:GENeral:STZero {{ON | 1} | {OFF | 0}}
Where N identifies a specific trace and must be selected from 1 to 128 {1:128}.
Query Syntax
:NETWorks:TRACeN:THReshold:GENeral:STZero?
Query Response
{1 | 0}
Description
When you select the ± Hysteresis threshold definition for the selected signal (see :NETWorks:TRACe:THReshold:GENeral:METHod), you can turn ON the :NETWorks:TRACe:THReshold:GENeral:STZero setting to move thresholds within ±10 mV to zero. This feature is useful for differential signals.