:NETWorks:TRACe:THReshold:GENeral:LOWer

Command Syntax

:NETWorks:TRACeN:THReshold:GENeral:LOWer  <amplitude>

<amplitude> is a double.

Where N identifies a specific trace and must be selected from 1 to 128 {1:128}.

Query Syntax

:NETWorks:TRACe{1:128}:THReshold:GENeral:LOWer?

Description

For the indicated S-parameter trace, sets or queries the General threshold's custom lower-threshold definition level. This command is used when making measurements with custom threshold definitions that are based on absolute amplitude. Before using this command,

Use the :NETWorks:TRACe:THReshold:GENeral:MIDDle command to enter a middle threshold level. Use the :NETWorks:TRACe:THReshold:GENeral:UPPer command to enter a upper threshold level.

The custom lower-threshold setting can be set from the front panel by choosing Measure > Thresholds... and in the Thresholds tab, General subtab of the Configure Measurements dialog box, setting the signal's Top-Base Definition.

Depending on the waveform type, specify the level in the units shown in the following table.

Units Used for Displayed Content Window Graphs
Content Window Graphs Y-Axis
Units
S-Parameters
Freq-Mag Decibels
Phase Degrees
GrpDelay Seconds