:NETWorks:TRACe:THReshold:GENeral:PMIDdle

Command Syntax

:NETWorks:TRACeN:THReshold:GENeral:PMIDdle  <percent>

Where <percent> is a decimal number from -25.0 to +125.0.

Where N identifies a specific trace and must be selected from 1 to 128 {1:128}.

Query Syntax

:NETWorks:TRACeN:THReshold:GENeral:PMIDdle?

Description

When the threshold method is a custom PERCent between top and base (see :NETWorks:TRACe:THReshold:GENeral:METHod), the :NETWorks:TRACe:THReshold:GENeral:PMIDdle command sets or queries the custom middle percent value.

Example Command Sequence

:NETWorks:TRACe2:THReshold:GENeral:TRACking OFF
:NETWorks:TRACe2:THReshold:GENeral:METHod PERCent
:NETWorks:TRACe2:THReshold:GENeral:PUPPer 125E-3
:NETWorks:TRACe2:THReshold:GENeral:PMIDdle 0E0
:NETWorks:TRACe2:THReshold:GENeral:PLOWer -125E-3