:NETWorks:TRACe:THReshold:RFALl:PUPPer
Command Syntax
:NETWorks:TRACeN:THReshold:RFALl:PUPPer <percent>
<percent> is a decimal number from -25.0 to +125.0.
Where N identifies a specific trace and must be selected from 1 to 128 {1:128}.
Query Syntax
:NETWorks:TRACeN:THReshold:RFALl:PUPPer?
Description
When the threshold method is a custom PERCent between top and base (see :NETWorks:TRACe:THReshold:RFALl:METHod), the :NETWorks:TRACe:THReshold:RFALl:PUPPer command sets or queries the custom upper percent value.
Example Command Sequence
:NETWorks:TRACe2:THReshold:RFALl:TRACking OFF :NETWorks:TRACe2:THReshold:RFALl:METHod PERCent :NETWorks:TRACe2:THReshold:RFALl:PUPPer 125E-3 :NETWorks:TRACe2:THReshold:RFALl:PLOWer -125E-3