:NETWorks:TRACe:THReshold:RFALl:METHod

Command Syntax

:NETWorks:TRACeN:THReshold:RFALl:METHod  {P1090 | P2080 | PERCent | ABSolute}

Where N identifies a specific trace and must be selected from 1 to 128 {1:128}.

Query Syntax

:NETWorks:TRACeN:THReshold:RFALl:METHod?

Description

Selects the upper, middle, and lower waveform threshold definitions using the following arguments:

P1090
Specifies threshold levels as 10% and 90% values between top and base.
P2080
Specifies threshold levels as 20% and 80% values between top and base.
PERCent
Specifies thresholds as custom percentages between top and base. To specify the percent values for the upper, middle, and lower thresholds, use the :NETWorks:TRACe:THReshold:RFALl:PUPPer and :NETWorks:TRACe:THReshold:RFALl:PLOWer commands.
ABSolute
Specifies thresholds as absolute upper, middle, and lower vertical values. To specify the values, use the :NETWorks:TRACe:THReshold:RFALl:UPPer and :NETWorks:TRACe:THReshold:RFALl:LOWer commands.
Selects custom user-defined threshold definitions based on absolute unit amplitudes.

Example Command Sequence

:NETWorks:TRACe2:THReshold:RFALl:TRACking OFF
:NETWorks:TRACe2:THReshold:RFALl:METHod ABSolute
:NETWorks:TRACe2:THReshold:RFALl:UPPer 125E-3
:NETWorks:TRACe2:THReshold:RFALl:LOWer -125E-3