:NETWorks:TRACe:THReshold:RFALl:TRACking

Command Syntax

:NETWorks:TRACeN:THReshold:RFALl:TRACking  {{ON | 1} | {OFF | 0}}

Where N identifies a specific trace and must be selected from 1 to 128 {1:128}.

Query Syntax

:NETWorks:TRACeN:THReshold:RFALl:TRACking?

Query Response

{1 | 0}

Description

Specifies whether a signal tracks the Rise/Fall threshold's global threshold definition or uses its own threshold definition.

The global threshold definition is set using the :MEASure:THReshold:RFALl commands (see Threshold Configuration Commands).

Example Command Sequence

:NETWorks:TRACe2:THReshold:RFALl:TRACking OFF
:NETWorks:TRACe2:THReshold:RFALl:METHod ABSolute
:NETWorks:TRACe2:THReshold:RFALl:UPPer 125E-3
:NETWorks:TRACe2:THReshold:RFALl:LOWer -125E-3