:NETWorks:TRACe:THReshold:GENeral:HYSTeresis
Command Syntax
:NETWorks:TRACeN:THReshold:GENeral:HYSTeresis <plus_or_minus_value>
<plus_or_minus_value> is a double.
Where N identifies a specific trace and must be selected from 1 to 128 {1:128}.
Query Syntax
:NETWorks:TRACeN:THReshold:GENeral:HYSTeresis?
Description
When the :NETWorks:TRACe:THReshold:GENeral:METHod setting is HYSTeresis, this command sets the user-defined ±hysteresis value for the waveform source.
Use the :NETWorks:TRACe:THReshold:GENeral:MIDDle command to enter the center threshold level.