:NETWorks:TRACe:THReshold:GENeral:MIDDle

Command Syntax

:NETWorks:TRACeN:THReshold:GENeral:MIDDle  <amplitude>

<amplitude> is a double.

Where N identifies a specific trace and must be selected from 1 to 128 {1:128}.

Query Syntax

:NETWorks:TRACe{1:128}:THReshold:GENeral:MIDDle?

Description

For the indicated S-parameter trace, sets or queries the custom middle-threshold definition level. This command is used when making measurements with custom threshold definitions that are based on absolute amplitude. Before using this command,

Use the :NETWorks:TRACe:THReshold:GENeral:UPPer command to enter a upper threshold level. Use the :NETWorks:TRACe:THReshold:GENeral:LOWer command to enter a lower threshold level.

The custom middle-threshold setting can be set from the front panel by choosing Measure > Thresholds... and selecting the Thresholds tab, General subtab in the Configure Measurements dialog box.

Depending on the waveform type, specify the level in the units shown in the following table.

Units Used for Displayed Content Window Graphs
Content Window Graphs Y-Axis
Units
S-Parameters
Freq-Mag Decibels
Phase Degrees
GrpDelay Seconds