:NETWorks:TRACe:THReshold:GENeral:TRACking
Command Syntax
:NETWorks:TRACeN:THReshold:GENeral:TRACking {{ON | 1} | {OFF | 0}}
Where N identifies a specific trace and must be selected from 1 to 128 {1:128}.
Query Syntax
:NETWorks:TRACeN:THReshold:GENeral:TRACking?
Query Response
{1 | 0}
Description
Specifies whether a signal tracks the General threshold's global threshold definition or uses its own threshold definition.
The global threshold definition is set using the :MEASure:THReshold:GENeral commands (see Threshold Configuration Commands).
Example Command Sequence
:NETWorks:TRACe2:THReshold:GENeral:TRACking OFF :NETWorks:TRACe2:THReshold:GENeral:METHod ABSolute :NETWorks:TRACe2:THReshold:GENeral:UPPer 125E-3 :NETWorks:TRACe2:THReshold:GENeral:MIDDle 0E0 :NETWorks:TRACe2:THReshold:GENeral:LOWer -125E-3