The Phase Noise application measures the phase noise of a DUT's output signal within a specified offset frequency range.
In this topic:
Absolute Phase Noise measurements
AM noise measurement
Spur identification and removal
Automatic carrier search
Segment Sweep
How to start Phase Noise |
|
Using Hardkey/SoftTab/Softkey |
Using a mouse |
|
|
The Phase Noise application measures the power density of the noise sideband relative to the power of the carrier over a start/stop offset frequency. The offset frequency corresponds to the distance from the carrier frequency. The log-transformed phase noise is displayed in dBc/Hz.
The bottom of the display area shows the carrier frequency, carrier power, and the Phase Noise start and stop offset frequencies.
The carrier power is measured by RF detector. If the harmonics of the DUT affect the power level measurement (for example, when measuring rectangle waves), SSA-X allows you to display the power level of the IF signal next to carrier power level. You can enable this option in the Preferences settings.
The x-axis is the offset frequency range displayed on a logarithmic scale to allow viewing the full offset range.
If the sweep time is greater than 2 seconds, a sweep indicator is displayed at the bottom of the display area to provide sweep time percentage complete:

Noise tables showing Spurious, Integrated Noise, and Spot Noise data can be displayed below the trace area.
This shows the number of current cross correlation averages for each offset frequency segment

When the correlation reaches the end point, the back color is turned to black.