Notes
|
Added Import Power Cal and Source PMax Table Cal in Power Cal Setting
Updated Save Data As dialog
Updated Power Cal Settings dialog
Added Burst Mode to the Optimizer Setup dialog for creating modulation files
Updated Banded 2D Calibration:
Banded System Measurement Setup
Added Millimeter Source Linearity Cal to Banded Installation Calibration
Updated Hybrid Source Calibration:
This help includes: Example Setup for U7229x Amplifier Control
Updated Modulation Properties dialog for Spectrum Analyzer and Modulation Distortion applications
and for E5081A.
Added phase stitching type, export raw data and show ADC range in MOD setup.
Added Operating Gain and updated descriptions of power traces in Distortion Measurement Parameters
Isolation Calibration is available in 2 port calibration using a mechanical cal kit.
Smith Chart can be displayed during Noise Figure Calibration
Ecal Temperature Query
Generic Ecal Control commands which supports multi-port Ecal (over 4 ports)
Added capability to turn off noise receiver pulling during calibration
Added support for importing Python files into the equation editor
(See also, Equation Editor and Python)
(E5080B, E5081A) Preference: Factory Calibration can be turned off at default
Code Emulator for E5071C supports the customized returned value for *OPT?.
Include Loss in TDR fixture compensation
Bug fix only
DUT SNP simulation for SMC and GCA /GCX (Simulator only)
ECal emulation on VNA simulator (Simulator only)
Support the E5081A (Support the E5081A for the simulator as well).
Suppot the E5080B-190 Vector Signal Analysis
(S96111B) Support Active Hot Parameter for E5080B, E5081A
(S96200B-Licensed Feature) Added a Hybrid Source driver, which combines a source and a mixer to create a high-frequency source. This new driver selection appears the External Device Configuration dialog.
Support the S96087B IMD (Intermodulation distortion measurements)
Support the S96024B Basic Pulsed-RF Measurements Lite
Support the Core Software
Modulation Distortion Enhancements:
IMD Multiple Receiver Configurations [requires active Option S9x087A/B KeysightCare subscription]
Actual Wave and 8-term error correction method in IMD/IMDX [requires active Option S9x087A/B KeysightCare subscription]
Multi-sensor Power Calibration for SMC/GCX [requires active Option S93082B, S93083B, or S93086B KeysightCare subscription]
Added four new Windows types for TDR [requires active Option S93010B or S93011B KeysightCare subscription]
Cal Update [Licensed Feature]
Support N755xA ECal modules
Support L8990M Switch matrix [Licensed Feature]
Modulation Distortion
Add support for 8-term correction
Window Type added to Time Domain Setup dialog [Licensed Feature]
Save/Load mixer files in CSV format [Licensed Feature]
Support for U1832A/B/C/D and U1833A/B/C/D Noise Sources [Licensed Feature]
Change the Fixture Generator Calculation Order
Some bug fixes
Support S96041B Impedance Analysis (E5080B)
Pulse Measurements in SA mode
Support Noise Figure Converter for S96029A/B(E5080B)
Support Gain Compression Converter for S96086A/B (E5080B)
Support S9x015B Real-time S-Parameter and Power Measurement Uncertainty (E5080B)
Support S9x460B Integrated True Mode Stimulus Application (E5080B)
Enhance the Fixture Simulator
Add Application IO GUI and commands (CONT:SING:AIO:PIN:CHAN:FUNC and CONT:SING:AIO:PIN:CHAN:FUNC:CAT) (E5080B)
Add CONT:HAND:IND:LOG to set the logic of the index signal. (E5080B)
Add Log Y-Axis and Complex Graph
Support Data Viewer
Support Multiport Calibration Assistant
Support S9xxxxB application software for floating/USB portable licenses.
Support Cal Pods
Support U205xXA/U206xXA Series USB Power Sensors.
Support the following items in the spectrum analysis.
Noise Power Ratio (NPR) measurement
Coherent Averaging Tab
Pulsed SA (Trigger & Pulse Tab, Pulse settings in source Tab)
Dual Band Configuration in advance tab
SA analysis marker
Supports E5080B.
Noise Figure Option S93027B (directly control mechanical tuners)
Support for U205xXA/U206xXA Series USB Power Sensors
Support for new Low Frequency Extension options
Banded millimeter wave installation calibration
Support for Windows 10
Active Hot Parameters application (Option S93110A/B, S93111A/B)
Support for Windows 10 operating system
Multi-dimensional sweep on a spectrum analyzer channel
SCPI
COM
Automatic Fixture Removal (AFR) SCPI commands
Maximum channels increased to 500
Added ISegment3 and ISegments6 interface commands
N5290A/N5291A Broadband Network Analyzer
Low Frequency Extension (Option 205/425)
Spectrum Analyzer Coherence and Data export features
Modernized Graphical User Interface
Tabbed soft panel enabling quick access to desired functions
Easily make complex setups and calibrations using Wizards
Marker Search
Unique limit test functions
Spectrum Analyzer enhanced features
Power Range SCPI and COM commands
SA Gated Measurement Quick Setup
Vector Signal Analyzer
SA broadband and banded millimeter-wave measurements
Cal All for millimeter wave measurement classes
Support for UXG signal generators
Narrowband Compensation to Noise Figure measurements
CPM Direct Receiver Calibration
New N5249A PNA-X model (Configuration | Specs)
Move App to Back
Equation Editor enhancements
Delta Match Calibration required on ALL N5231A, N5232A, and N5239A models.
Unguided TRL Cal allowed on all PNA 4-port models
New N523xA models
New External Device configuration:
IMSpectrum in mmWave
May 2013: Support for U2020X Power Sensors
New N522x Models
"Src 2 out Port 2" factory configuration on PNA-X Opt 423.
Use a Power Table with mmWave SMC Measurements
mmWave; Mixer mode - 2-port test set on 4-port PNA
Source Phase Control - Opt 088
FCA Update - Opt 082, and 083
2-Port and 4-Port Fixture Extrapolation and Reverse Ports.
Phase Coherent "R over R" measurements
Tip - Do you access the same PNA dialog often? Your Favorites are always two keystrokes away. |
N5247A - 67 GHz PNA-X
IF Gain Setting
Receiver Overload/Compression Warning and Power OFF Preferences
Integrated Pulse Measurements (Opt 008)
Noise Figure using Standard PNA Receiver (Opt 028)
Noise Figure on N5244A/45A (Opt H29)
Edge and Level Trigger in Pulse
Include Phase with SMC (PNA-X with Opt 083)
Fixturing in Apps
Max Output Power for GCA (Opt 086)
Mechanical Device conflicts cause Channel Block (NOT Channel Hold)
Fixture Power Compensation
Data Save Enhancements
Characterize Adaptor Macro Rev. A.02.10
Reverse S2P
Load the PNA Power Loss Table from an existing S2P file
Power Meter as Receiver (PMAR)
Device side USB
Limited Port Mapping on IMD
SMC Measurements with mmWave Modules
mmWave Measurements with no Test Set
New 40 GHz and 50 GHz PNA-X Models
New 13.5 GHz PNA-X Model
Phase Sweep in iTMSA
Noise Figure App enhancements:
MM Module enhancements:
Power Level Control
Supports iTMSA
New N5264A model
IMD Application (Opt 087)
Characterize Adaptor Macro 2.0
Support for N5261A and N5262A MM test sets
cXL Code Translation Software - Quick Link