:CALibrate:DARK:CHANnel:STATus:TEMPerature?
Command:
Deprecated
Flex Apps:
FlexDCA
Deprecated command. For FlexDCA revision A.01.70 and above, use the :CALibrate:DARK:CHAN:STATus:DTEMperature? command.
Query Syntax
:CALibrate:DARK:CHANnel{N}:STATus:TEMPerature?
{N} identifies a specific channel and must be selected from {1:8}{A|B|C|D}. For example, 3C.
Description
Queries the N1000A's change in temperature from the time when the last dark calibration was performed on the indicated channel. A calibration should be performed if the change in N1000A temperature exceeds ±5°C. Use the CHANnel{N}:STARt command to start a dark calibration.
Example Returned Status String
"-6.10"
Example Command
:CALibrate:DARK:CHAN3A:STATus:TEMPerature?