:CALibrate:TIMebase:SLOT:CHANnel
Instruments:
N1092
Flex Apps:
FlexDCA
Command Syntax
:CALibrate:TIMebase:SLOT{1:8}:CHANnel CHAN{1:8}A
Where the required specifier {1:8} identifies a specific N1092 module by slot.
Query Syntax
:CALibrate:TIMebase:SLOT{1:8}:CHANnel?
Query Response
CHAN{1:8}{A|B|C|D}
Description
Selects the N1092x's electrical channel to be used for a N1092 Timebase Calibration. The only allowable channel is channel A. The calibration requires that a 26.000000 GHz clock signal be connected to the N1000A's input channel that is specified with this command. To start the calibration, use the :CALibrate:TIMebase:SLOT:STARt command.
Requires FlexDCA revision A.06.00 and above.
Example Command
:CALibrate:TIMebase:SLOT3:CHANnel CHAN3A