:CALibrate:TIMebase:SLOT:STATus:DETails?
Instruments:
N1092
Flex Apps:
FlexDCA
Query Syntax
:CALibrate:TIMebase:SLOT{1:8}:STATus:DETails?
Where the required specifier {1:8} identifies a specific N1092 module by slot.
Description
Returns a string that provides the date of the last timebase calibration for the indicated slot as well as the elapsed time and the temperature (Celsius) change. Use the :CALibrate:TIMebase:SLOT:STATus? parent query to determine if a calibration is needed and how the calibration is made.
The following is an example of the returned string:
"Time of last Calibration: 01/08/2014 07:07:12,Elapsed Calibration Time: 8 days,Temperature Change: 1.73 C"
Requires FlexDCA revision A.03.00 and above.
Example Command
:CALibrate:TIMebase:SLOT3:STATus:DETails?