:CALibrate:TIMebase:SLOT:STATus:DTEMperature?
Instruments:
N1092
Flex Apps:
FlexDCA
Query Syntax
:CALibrate:TIMebase:SLOT{1:8}:STATus:DTEMperature?
Where the required specifier {1:8} identifies a specific N1092 module by slot.
Description
Returns a string that provides the change in temperature (Celsius) from the last slot timebase calibration. Use the :CALibrate:TIMebase:SLOT:STATus? parent query to determine if a calibration is needed and how the calibration is made.
The following is an example of the returned string, which indicates that the temperature of the N1000A has risen 1.73°C:
"1.730000000E+00"
Requires FlexDCA revision A.03.00 and above.
Example Command
:CALibrate:TIMebase:SLOT3:STATus:DTEMperature?