:CALibrate:TIMebase:SLOT:STATus:TIME?
Instruments:
N1092
Flex Apps:
FlexDCA
Query Syntax
:CALibrate:TIMebase:SLOT{1:8}:STATus:TIME?
Where the required specifier {1:8} identifies a specific N1092 module by slot.
Description
Returns a string that provides the time that has elapsed since the last slot timebase calibration. Use the :CALibrate:TIMebase:SLOT:STATus? parent query to determine if a calibration is needed and how the calibration is made.
The following is an example of the returned string:
"01/09/2014 06:20:09"
Requires FlexDCA revision A.03.00 and above.
Example Command
:CALibrate:TIMebase:SLOT3:STATus:TIME?