:CALibrate:TIMebase:SLOT:STATus?
Instruments:
N1092
Flex Apps:
FlexDCA
Query Syntax
:CALibrate:TIMebase:SLOT{1:8}:STATus?
Where the required specifier {1:8} identifies a specific N1092 module by slot.
Query Response
{CALIBRATED | UNCALIBRATED}
Description
Returns the status of the timebase calibration for the module installed in the indicated slot. Use the :CALibrate:TIMebase:SLOT:STATus:DETails, :CALibrate:TIMebase:SLOT:STATus:DTEMperature, and :CALibrate:TIMebase:SLOT:STATus:TIME child commands to return detailed information about the calibration status. Use the :CALibrate:TIMebase:SLOT:STARt command to start a timebase calibration.
Requires FlexDCA revision A.03.00 and above.
Example Command
:CALibrate:TIMebase:SLOT3:STATus?