:CHANnel:DISPlay
Flex Apps:
FlexDCA
FlexRT
Command Syntax
:CHANnel{1:8}{A|B|C|D}:DISPlay {ON | OFF | 1 | 0}
Where the required specifier {1:8}{A|B|C|D} identifies a channel by its module slot number and channel letter. For example, channel 3C (CHANnel3C).
The channel specifier will fail if it does not include a slot number. If instead the suffix's channel letter is missing, the command defaults to letter A. As a result, the best practice is to always explicitly specify the channel by including both the module slot number and channel letter.
Query Syntax
:CHANnel{1:8}{A|B|C|D}:DISPlay?
Query Response
{1 | 0}
Description
Turns the display of the specified channel on or off. Use the :CHANnel:STATus command to determine if a channel is available for display.
Example Command
:CHANnel2A:DISPlay ON