:DIFF:COPY
Command Syntax
:DIFF{1:8}{A|C}:COPY {DIFF{1:8}{A|C}}
Where the required specifier {1:8}{A|C} identifies the destination channel into which settings are copied. For example, :DIFF2A.
Where the required command argument {DIFF{1:8}{A|C}} identifies a source channel from which to copy the settings. For example, DIFF2C.
The channel specifier will fail if it does not include a slot number. If instead the suffix's channel letter is missing, the command defaults to letter A. As a result, the best practice is to always explicitly specify the channel by including both the module slot number and channel letter.
Description
Copies channels settings from a source channel into the destination channel. Copied settings include the following:
- Scale
- Offset
- Hardware Skew
- Software Delay
- Signal Type Auto Detect and Type
- External Transducer settings
- External Attenuator settings
The copied settings do not include waveform color or any custom waveform name.
Requires FlexDCA revision A.06.50 and above.
Example Command
:DIFF2A:COPY DIFF2B