:DIFF:DISPlay

Instrument:
N1000A
DCA-M
Flex Apps:
FlexDCA
FlexRT
Meas. mode:
Scope
Eye
Jitter
TDR
Waveform type:
Differential

Command Syntax

:DIFF{1:8}{A|C}:DISPlay {ON | OFF | 1 | 0}

Where the required specifier {1:8}{A|C} identifies the differential channel by its module slot and channel letter. For example, the differential waveform of channels 1A and 1B would be identified as :DIFF1A.

The channel specifier will fail if it does not include a slot number. If instead the suffix's channel letter is missing, the command defaults to letter A. As a result, the best practice is to always explicitly specify the channel by including both the module slot number and channel letter.

Query Syntax

:DIFF{1:8}{A|C}:DISPlay?

Query Response

{1 | 0}

Description

Turns the display of the specified differential channel on or off. Use the STATus command to determine if a differential channel is available for display. Use the DMODe command to enable a differential waveform.

Example Command Sequence

:DIFF1A:DEMODe ON
*OPC?
…  //  Your code to synchronize execution timing.
:DIFF1A:DISPlay ON