:DIFF:FCHan?
Instrument:
N1000A
DCA-M
Flex Apps:
FlexDCA
FlexRT
Meas. mode:
Scope
Eye
Jitter
Waveform type:
Differential
Query Syntax
:DIFF{1:8}{A|C}:FCHan?
Where the required specifier {1:8}{A|C} identifies the differential channel by its module slot and channel letter. For example, the differential waveform of channels 1A and 1B would be identified as :DIFF1A.
The channel specifier will fail if it does not include a slot number. If instead the suffix's channel letter is missing, the command defaults to letter A. As a result, the best practice is to always explicitly specify the channel by including both the module slot number and channel letter.
Description
Queries the first source of a differential signal. For example, CHAN1A. Use the :DIFF:SCHan query to determine the second source of a differential signal.
Example Command
:DIFF2A:FCHan?