:DISK:JSANalysis:FNAMe:AUPDate
Meas. mode:
Scope
Eye
Jitter
Feature:
JSA
Waveform type:
NRZ
PAM4
Flex Apps:
FlexDCA
Command Syntax
:DISK:JSANalysis:FNAMe:AUPDate
Description
Increments a file name's autonumber for the next file saved with the :DISK:JSANalysis:SAVE command. The autonumber format is explained in :DISK:JSANalysis:FNAMe.
Requires FlexDCA revision A.05.70 and above.
Example Command Sequence
:DISK:JSANalysis:FNAMe "my_file_1" :DISK:JSANalysis:SAVE # my_file_1.jsax … … :DISK:JSANalysis:FNAMe:AUPDate :DISK:JSANalysis:SAVE # my_file_2.jsax