:DISK:JSANalysis:FNAMe:USTandard
Meas. mode:
Scope
Eye
Jitter
Feature:
JSA
Waveform type:
NRZ
PAM4
Flex Apps:
FlexDCA
FlexRT
FlexPLL
Command Syntax
:DISK:JSANalysis:FNAMe:USTandard
Description
Resets the file name for the JSA analysis file from using a custom name to using the standard name in the following form:
JSAData_<date><autonumber>.<extension>
For example, JSAData_2020-10-23_1.jsax. Refer to :DISK:JSANalysis:FNAMe to learn about standard and custom names.
Requires FlexDCA revision A.05.70 and above.