:DISK:JSANalysis:RECall
Meas. mode:
Scope
Eye
Jitter
Feature:
JSA
Waveform type:
NRZ
PAM4
Flex Apps:
FlexDCA
JSA requires an 86108A/B module with Option JSA. To use JSA in Jitter Mode, the Research and Development package is required.
Command Syntax
:DISK:JSANalysis:RECall
Description
Loads a Jitter Spectrum Analysis (JSA) database file into FlexDCA's one available JSA memory. Use the :DISK:JSANalysis:FNAMe command to specify the file to load. Since there is only one JSA memory, the :DISK:JSANalysis:RECall:DESTination command always points to CRAMemory.
Requires FlexDCA revision A.02.50 and above.