:DISK:JSANalysis:SAVE
Meas. mode:
Scope
Eye
Jitter
Feature:
JSA
Waveform type:
NRZ
PAM4
Flex Apps:
FlexDCA
FlexRT
FlexPLL
JSA requires an 86108A/B module with Option JSA. To use JSA in Jitter Mode, the Research and Development package is required.
Command Syntax
:DISK:JSANalysis:SAVE
Description
Saves the Jitter Spectrum Analysis (JSA) database to a file. Use the :DISK:JSANalysis:FNAMe command to specify the file name. To increment the automatic file number index, use the :DISK:JSANalysis:FNAMe:AUPDate command.
To load a jitter database file into one of FlexDCA's eight eye memories using the :JSAMemory:RECall and :JSAMemory:RECall:DESTination commands.
Requires FlexDCA revision A.02.50 and above.
Example Command Sequence
:DISK:JSANalysis:FNAMe "%USER_DATA_DIR%\Jitter Data\myfile" :DISK:JSANalysis:SAVE
Related Commands
:DISK:JSANalysis:FNAMespecifies the saved file's name.:DISK:JSANalysis:FNAMe:AUPDateupdates autonumber, if used.:DISK:JSANalysis:FNAMe:USTandardresets to the standard file name.:DISK:JSANalysis:RECallspecifies the type of file saved.:DISK:JSANalysis:RECall:DESTinationspecifies the source waveform on which to perform the measurement.