:DISK:JSANalysis:RECall:DESTination
Meas. mode:
Scope
Eye
Jitter
Feature:
JSA
Waveform type:
NRZ
PAM4
Flex Apps:
FlexDCA
JSA requires an 86108A/B module with Option JSA. To use JSA in Jitter Mode, the Research and Development package is required.
Command Syntax
:DISK:JSANalysis:RECall:DESTination CRAMemory
Query Syntax
:DISK:JSANalysis:RECall:DESTination?
Description
Selects the target Jitter Spectrum Analysis (JSA) memory location to load a waveform memory file. Since there is only one JSA memory location, the only valid argument for this command is CRAMemory. Use the :DISK:JSANalysis:RECall command to actually load the file into the jitter database.
Requires FlexDCA revision A.02.50 and above.