:DISPlay:WINDow:FDLegend
Command Syntax
:DISPlay:WINDow:FDLegend {OFF | ON}
Query Syntax
:DISPlay:WINDow:FDLegend?
Description
Shows or hides the Signals identification legend on all frequency-domain windows. This label is displayed in the content window's upper-right corner. The legend identifies TDR Mode S-parameters and the output of the FFT function in GrpDelay, Freq-Mag, and Phase content windows.
For the legend on the time-domain waveforms, Time-Volts, Time-%, and Time-Ohms, use the :DISPlay:WINDow:TDLegend command.
Requires FlexDCA revision A.03.00 and above.