:DISPlay:WINDow:T:VOLTs:LEGend:EXPand
Command Syntax
:DISPlay:WINDow:T:VOLTs{N}:LEGend:EXPand {ON | OFF}
{N} identifies a widow {1:4}.
Query Syntax
:DISPlay:WINDow:T:VOLTs{N}:LEGend:EXPand?
Description
Expands or contracts the Signals legend that is shown in the Time-Volts waveform content window. To completely remove the signal legend from all time-domain windows, use the :WINdow:TDLegend command.
Requires FlexDCA revision A.04.00 and above.