:DISPlay:WINDow:ECLegend
Package License:
L-RND
License:
401
Command Syntax
:DISPlay:WINDow:ECLegend {OFF | ON}
Query Syntax
:DISPlay:WINDow:ECLegend?
Description
Shows or hides the Eye Contours identification legend on the Waveform window. If multiple channels waveforms are shown with legends all of the displayed legends are controlled by this setting. The legend identifies the individual eye contour lines on a waveform. To expand or contract all displayed eye contour legends, use the :DISPlay:WINDow:TIME:LEGend:ECEXpand command. Use the commands in the :ECONtour subsystem to create and display contour lines. If Option 200, Enhanced Jitter Analysis, is also installed, the application leverages the DCA-X's ability to measure ultra-low levels of Random Jitter (RJ). This can be used to obtain fixed RJ values.
Requires FlexDCA revision A.05.30 and above.