:DISPlay:WINDow:TIME:LEGend:ECEXpand
Package License:
L-RND
License:
401
Command Syntax
:DISPlay:WINDow:TIME:LEGend:ECEXpand {ON | OFF}
Query Syntax
:DISPlay:WINDow:TIME:LEGend:ECEXpand?
Description
Expands or contracts all displayed Eye Contours legends that are shown in the Waveform content window. To display or hide the Eye Contours legend, use the :DISPlay:WINDow:ECLegend command. Use the commands in the :ECONtour subsystem to create and display contour lines. If Option 200, Enhanced Jitter Analysis, is also installed, the application leverages the DCA-X's ability to measure ultra-low levels of Random Jitter (RJ). This can be used to obtain fixed RJ values.
Requires FlexDCA revision A.05.30 and above.