:DISPlay:WINDow:TDLegend
Command Syntax
:DISPlay:WINDow:TDLegend {OFF | ON}
Query Syntax
:DISPlay:WINDow:TDLegend?
Description
Shows or hides the Signals identification legend on all time-domain windows. This label is displayed in the content window's upper-right corner. The legend identifies:
- Channel waveforms in the Waveform content window.
- TDR Mode time-domain parameters in Time-Volts, Time-%, and Time-Ohms content windows.
For the legend on the frequency-domain waveforms, GrpDelay, Freq-Mag, and Phase, use the :DISPlay:WINDow:FDLegend command.
Requires FlexDCA revision A.03.00 and above.