:DISPlay:TSMode
Instrument:
N1000A
DCA-M
Meas. mode:
Scope
Eye
Jitter
TDR
Flex Apps:
FlexDCA
FlexRT
Command Syntax
:DISPlay:TSMode {MINimized | HSIZe | FSIZe}
Query Syntax
:DISPlay:TSMode?
Description
Sets the height of all displayed secondary panels that are shown below the waveform gratical. Examples of secondary panels include the measurement Results, Marker, and Histogram panels. These panels can be hidden (MINimized), full vertical height (FSIZe), or half vertical height (HSIZe). The query form of the command returns the current panel state.
Minimizing the height is the same as clicking the expander arrow that is above the panels.
Requires FlexDCA revision A.05.40 and above.