:EMEMory:XSCale?
Instrument:
N1000A
N109x
UXR Scope
Flex Apps:
FlexDCA
FlexRT
Meas. mode:
Eye
Waveform type:
NRZ
PAM4
Query Syntax
:EMEMory{1:8}:XSCale?
Where the required specifier {1:8} identifies one of eight eye memories.
Description
Queries the horizontal timebase scale (seconds-per-division or symbols displayed) that is stored in eye-memory. It may or may not be the same as FlexDCA's current setting. Query the units (seconds or symbols) with :EMEMory:XUNits?.
Example Command
:EMEMory3:XSCale?