:EMEMory:YSCale?
Instrument:
N1000A
N109x
UXR Scope
Flex Apps:
FlexDCA
FlexRT
Meas. mode:
Eye
Waveform type:
NRZ
PAM4
Query Syntax
:EMEMory{1:8}:YSCale?
Where the required specifier {1:8} identifies one of eight eye memories.
Description
Queries the vertical scale (sensitivity) stored for the waveform in eye-memory. This is volts-per-division for electrical waveforms and watts-per-division for optical waveforms. It may or may not be the same as FlexDCA's current setting. The vertical expansion and contraction is about the center offset value (:EMEMory:YOFFset) stored in eye memory and not at the ground reference. For optical channels, vertical expansion and contraction is about the second graticule division from the bottom of the display screen and also not at the ground reference.
Example Command
:EMEMory3:YSCale?