:EMEMory:YTOP?
Instrument:
N1000A
N109x
UXR Scope
Flex Apps:
FlexDCA
FlexRT
Meas. mode:
Eye
Waveform type:
NRZ
PAM4
Query Syntax
:EMEMory{1:8}:YTOP?
Where the required specifier {1:8} identifies one of eight eye memories.
Description
Queries the amplitude value stored in eye-memory that corresponds to the graticule's top edge. This is the value that existed when the source waveform was saved into eye memory or, if the data was loaded into eye memory from a color-grade gray-scale file (:DISK:EYE:SAVe), it is the value that existed when the file was created. It may or may not be the same as FlexDCA's current setting.
Example Command
:EMEMory3:YTOP?