:EMEMory:YOFFset?
Instrument:
N1000A
N109x
UXR Scope
Flex Apps:
FlexDCA
FlexRT
Meas. mode:
Eye
Waveform type:
NRZ
PAM4
Query Syntax
:EMEMory{1:8}:YOFFset?
Where the required specifier {1:8} identifies one of eight eye memories.
Description
Queries the voltage (or Watts) value representing the vertical offset that is stored for the waveform in eye-memory. The offset is located at the center of the display for electrical channels and the second graticule division from the bottom of the display screen for optical channels. It may or may not be the same as FlexDCA's current setting. The vertical scale for the waveform can be queried with :EMEMory:YSCale command.
Example Command
:EMEMory3:YOFFset?