:EMEMory:XUNits?
Instrument:
N1000A
N109x
UXR Scope
Flex Apps:
FlexDCA
FlexRT
Meas. mode:
Eye
Waveform type:
NRZ
PAM4
Query Syntax
:EMEMory{1:8}:XUNits?
Where the required specifier {1:8} identifies one of eight eye memories.
Description
Queries the horizontal units (SEConds or BIT) stored for the waveform in eye-memory. It may or may not be the same as FlexDCA's current setting.
Example Command
:EMEMory3:XSCale?