:JSAMemory:DISPlay
Instrument:
N1000A
N109x
UXR Scope
Flex Apps:
FlexDCA
FlexRT
Meas. mode:
Scope
Eye
Jitter
Waveform type:
NRZ
PAM4
Package License:
L-RND
L-SNT
Command Syntax
:JSAMemory:DISPlay {ON | OFF}
Query Syntax
:JSAMemory:DISPlay?
Description
Turn on or off the display of the JSA memory data. To import data into JSA memory from a file, use the :DISK:JSANalysis:RECall command.
JSA requires an 86108A/B module with Option JSA. To use JSA in Jitter Mode, L-RND package license (includes feature F-JIT Enhanced Jitter Analysis) is required.
Requires FlexDCA revision A.02.50 and above.