:LTESt:ACQuire:SWAVeform:CHANnel:WMEMory
Instrument:
N1010A
N1000A
DCA-M
Meas. mode:
Scope
Eye
Jitter
TDR
Flex Apps:
FlexDCA
FlexRT
Command Syntax
:LTESt:ACQuire:SWAVeform:CHANnel{1:8}{A|B|C|D}:WMEMory WMEMory{1:8}
Where the specifier {1:8}{A|B|C|D} identifies the channel.
Where the argument WMEMory{1:8} identifies a waveform memory.
Query Syntax
:LTESt:ACQuire:SWAVeform:CHANnel{1:8}{A|B|C|D}:WMEMory?
Description
Upon completion of an acquisition limit test, selects a waveform memory as a destination to save a channel waveform. Use the :LTESt:ACQuire:SWAVeform:CHAN:STATe command to enable and disable waveform reporting for the channel. To enable or disable acquisition limit tests, use the :LTESt:ACQuire:STATe command.
Example Command
:LTESt:ACQuire:SWAVeform:CHANnel3C:WMEMory WMEMory3