:LTESt:ACQuire:SWAVeform:DIFF:WMEMory
Instrument:
N1010A
N1000A
DCA-M
Meas. mode:
Scope
Eye
Jitter
TDR
Flex Apps:
FlexDCA
FlexRT
Command Syntax
:LTESt:ACQuire:SWAVeform:DIFF{1:8}{A|C}:WMEMory WMEMory{1:8}
Where {1:8}{A|C} identifies a differential channel.
Where the argument WMEMory{1:8} identifies a waveform memory.
Query Syntax
:LTESt:ACQuire:SWAVeform:DIFF{1:8}{A|C}:WMEMory?
Description
Specifies a waveform memory for saving a differential waveform as a reporting action for an acquisition limit test. Use the :LTESt:ACQuire:SWAVeform:DIFF:STATe command to enable and disable waveform reporting for the channel. To enable or disable acquisition limit tests, use the :LTESt:ACQuire:STATe command.
Example Command
:LTESt:ACQuire:SWAVeform:DIFF3A:WMEMory WMEMory3