:LTESt:ACQuire:SWAVeform:CMODe:STATe
Instrument:
N1010A
N1000A
Meas. mode:
TDR
Flex Apps:
FlexDCA
This command is compatible with TDR/TDT mode only.
Command Syntax
:LTESt:ACQuire:SWAVeform:CMODe{1:8}{A|C}:STATe {DISK | MEMory | OFF}
Where the specifier {1:8}{A|C} identifies a common-mode channel.
Query Syntax
:LTESt:ACQuire:SWAVeform:CMODe{1:8}{A|C}:STATe?
Query Response
{DISK | MEM | OFF}
Description
In TDR/TDT Mode, selects to save a common-mode waveforms to a file or memory after the limit test acquires the specified number of waveforms, samples, or patterns. Use the :LTESt:ACQuire:CTYPe command and its child commands to specify the test conditions required to end the test. To enable or disable acquisition limit tests, use the :LTESt:ACQuire:STATe command. The following command arguments are available:
- DISK
- Saves the waveform to a file. Use the
:LTESt:ACQuire:SWAVeform:CMODe:FNAMecommand to specify the file name. - MEMory
- Saves the waveform to a memory location. Use the
:LTESt:ACQuire:SWAVeform:CMODe:WMEMorycommand to specify the memory location. - OFF
- Turns off the saving of a common-mode waveform.
Requires FlexDCA revision A.04.00 and above.
Example Command
:LTESt:ACQuire:SWAVeform:CMODe1A:STATe DISK