:LTESt:ACQuire:SWAVeform:CMODe:WMEMory
Instrument:
N1010A
N1000A
Meas. mode:
TDR
Flex Apps:
FlexDCA
This command is compatible with TDR/TDT mode only.
Command Syntax
:LTESt:ACQuire:SWAVeform:CMODe{1:8}{A|C}:WMEMory
Where the specifier {1:8}{A|C} identifies a common-mode channel.
Where the argument WMEMory{1:8} identifies a waveform memory.
Query Syntax
:LTESt:ACQuire:SWAVeform:CMODe{1:8}{A|C}:WMEMory?
Description
In TDR/TDT Mode, specifies a waveform memory for saving a common-mode waveform as a reporting action for an acquisition limit test. Use the :LTESt:ACQuire:SWAVeform:CMODe:STATe command to enable and disable waveform reporting for the channel. To enable or disable acquisition limit tests, use the :LTESt:ACQuire:STATe command.
Requires FlexDCA revision A.04.00 and above.
Example Command
:LTESt:ACQuire:SWAVeform:CMODe3A:WMEMory WMEMory3