:LTESt:LLINe:SIMage:MONochrome
Instrument:
N1010A
N1000A
DCA-M
Meas. mode:
Scope
Eye
Jitter
TDR
Flex Apps:
FlexDCA
FlexRT
Command Syntax
:LTESt:LLINe:SIMage:MONochrome {ON | OFF}
Query Syntax
:LTESt:LLINe:SIMage:MONochrome?
Description
Upon completion of limit testing for a limit line test, a screen image can be saved to a graphics file. Use this command to turn monochrome screen capture on and off. When on, a black and white image will be captured and saved into a file specified by the :LTESt:LLINe:SIMage:FNAMe command. Selecting monochrome automatically inverts the graticule area's background color.
Use the :LTESt:LLINe:SIMage:STATe command to enable and disable screen-capture reporting. To enable or disable limit testing for a limit line test, use the :LTESt:LLINe:TEST:STATe command.
Requires FlexDCA revision A.04.50 and above.
Example Command
:LTESt:LLINe:SIMage:MONochrome ON