:LTESt:MTESt:SWAVeform:CHANnel:WMEMory
Instrument:
N1010A
N1000A
DCA-M
Meas. mode:
Scope
Eye
Jitter
TDR
Flex Apps:
FlexDCA
FlexRT
Command Syntax
:LTESt:MTESt:SWAVeform:CHANnel{1:8}{A|B|C|D}:WMEMory WMEMory{1:8}
Where the specifier {1:8}{A|B|C|D} identifies the channel.
Where the argument WMEMory{1:8} identifies a waveform memory.
Query Syntax
:LTESt:MTESt:SWAVeform:CHANnel{1:8}{A|B|C|D}:WMEMory?
Description
Upon completion of an mask limit test, selects a waveform memory as a destination to save a channel waveform. Use the :LTESt:MTESt:SWAVeform:CHAN:STATe command to enable and disable waveform reporting for the channel.