:LTESt:MTESt:SWAVeform:FUNCtion:STATe
Instrument:
N1010A
N1000A
DCA-M
Meas. mode:
Scope
Eye
Jitter
TDR
Flex Apps:
FlexDCA
FlexRT
Command Syntax
:LTESt:MTESt:SWAVeform:FUNCtion{1:64}:STATe {DISK | MEMory | OFF}
Where {1:64} identifies a function.
Query Syntax
:LTESt:MTESt:SWAVeform:FUNCtion{1:64}:STATe?
Query Response
{DISK | MEM | OFF}
Description
Saves a function waveform to a file after the mask limit test acquires the specified number of failures. Use the :LTESt:MTESt:MRESult:FAILures command to specify the number of failures required to end the test. Use the :LTESt:MTESt:SWAVeform:FUNCtion{1:64}:FNAMe command to specify the file name.
Example Command
:LTESt:MTESt:SWAVeform:FUNCtion2:STATe MEMory