:LTESt:MTESt:SWAVeform:CHANnel:STATe
Instrument:
N1010A
N1000A
DCA-M
Meas. mode:
Scope
Eye
Jitter
TDR
Flex Apps:
FlexDCA
FlexRT
Command Syntax
:LTESt:MTESt:SWAVeform:CHANnel{1:8}{A|B|C|D}:STATe {DISK | MEMory | OFF}
Where the specifier {1:8}{A|B|C|D} identifies the channel.
Query Syntax
:LTESt:MTESt:SWAVeform:CHANnel{1:8}{A|B|C|D}:STATe?
Query Response
{DISK | MEM | OFF}
Description
Saves a channel waveform to a file after the mask limit test acquires the specified number of failures. Use the :LTESt:MTESt:MRESult:FAILures command to specify the number of failures required to end the test. Use the :LTESt:MTESt:SWAVeform:CHANnel{1:8}{A|B|C|D}:FNAMe command to specify the file name.