:MEASure:ERATio:DCFactor

Meas. mode:
Eye
Waveform type:
NRZ
PAM
Flex Apps:
FlexDCA
FlexRT

Command Syntax

:MEASure:ERATio:DCFactor  {ON | OFF}

Query Syntax

:MEASure:ERATio:DCFactor?

Description

When an Extinction Ratio Correction Factor (ERCF) is applied, turns on or off the display of the ERCF values in the measurement results panel. The defaul setting is ON, which displays the ERCF factor value. To apply the extinction ratio factor, use the :MEASure:ERATio:ACFactor command. To enter an extinction ratio factor, use the :MEASure:ERATio:CFACtor command.

Display ERCF Values setting: On Display ERCF Values setting: Off

Query Response

{1 | 0}

Requires FlexDCA revision A.05.41 and above.