:MEASure:ERATio:WMEMory:ACFactor
Meas. mode:
Eye
Waveform type:
NRZ
Flex Apps:
FlexDCA
FlexRT
Command Syntax
:MEASure:ERATio:FUNCtionN:ACFactor {ON | OFF}
Where N identifies one of sixty four {1:64} math functions. For example, :FUNCtion2.
Query Syntax
:MEASure:ERATio:FUNCtionN:ACFactor?
Description
For an Eye/Mask mode extinction-ratio measurement, turns on the use of an Extinction Ratio Correction Factor (ERCF) on a math function. This command both selects the function and turns the ERCF on. To enter the actual ERCF value, use one of the following commands:
- NRZ waveform:
:MEASure:ERATio:FUNCtion:FACtor - PAM waveform:
:MEASure:ERATio:FUNCtion:OERFactor
To apply an extinction ratio correction factor to a channel, use the :MEASure:ERATio:CHANnel:ACFactor command.
To perform an extinction ratio measurement on an NRZ waveform, use the :MEASure:EYE:ERATio command. For a PAM4 waveform, use the :MEASure:EYE:OER command.
Requires FlexDCA revision A.07.50 and above.