:MEASure:ERATio:CHANnel:ACFactor
Meas. mode:
                                                Eye
                                            Waveform type:
                                                NRZ
                                            Flex Apps:
                                                FlexDCA
                                                FlexRT
                                            Command Syntax
:MEASure:ERATio:CHANnelN:ACFactor  {ON | OFF}
                                            Where N identifies a specific channel and must be selected from {1:8}{A|B|C|D}. For example, CHANnel3C.
Query Syntax
:MEASure:ERATio:CHANnelN:ACFactor?
                                            Description
For an Eye/Mask mode extinction-ratio measurement, turns on the use of an Extinction Ratio Correction Factor (ERCF) on a channel. This command both selects the channel and turns the ERCF on. To enter the actual ERCF value, use one of the following commands:
- NRZ waveform: 
:MEASure:ERATio:CHANnel:CFACtor - PAM waveform: 
:MEASure:ERATio:CHANnel:OERFactor 
To apply an extinction ratio correction factor to a math function, use the :MEASure:ERATio:FUNCtion:ACFactor command.
To perform an extinction ratio measurement on an NRZ waveform, use the :MEASure:EYE:ERATio command. For a PAM4 waveform, use the :MEASure:EYE:OER command.